11/14/2018 10:38 AM | |
Posts: 3 Rating: (0) |
Hi, I have to make some adjustments in an old PLC program which was created with TIA portal V13 SP1. However, my TIA portal V13 SP2 update 9 is constantly crashing when I try ANYTHING with winCC. Even with extremely simple (new) projects such as: Add device > PC station > add IE connection > add WinCC Rt advanced. (It crashes when adding the winCC RT) "The TIA portal has encountered a problem and needs to close." I've added a crash report of this as attachment. OS: Windows 10 pro 16299 I was adviced against upgrading the project to V14 or higher. Is there any fix for this? Attachment4651e689-1e87-43ed-9cc7-55173501e9c0.zip (36 Downloads) |
Follow us on