Industry Online Support
Technical Forum
11/17/2011 11:47 AM | |
Posts: 5 Rating: (0) |
Hi, Problem 01: I've set up 2 client workstations taking OS data straight from the servers (main and redundant). One client with all the licenses needed and another one without (still waiting for delivery). While everything is perfect on the licensed client, not so much for the other one. What I know, without client license, we can't view the archieved trending. Is alarm also affected by this? I transfered the licenses to the other client to check whether this is the cause but still no alarm reported in the WinCC runtime. Details as below: Development: PCS7 7.1 SP3, WinCC 7.0 + SP2 + Upd 4. Configuration: 1 ES, 2 Servers (main and redundant), 2 Clients The catch here is the OS and clients are configured for 2 different areas of the plant, one for each client. Each client is phobited to view the other area by using User Administrator tool in WinCC. I think the problem lies within here but I tried different authorization combination and still no avail. Any idea where to look at? problem 2 is splitted to SC library Thanks and Regards, Asdian |
Last edited by: O_Moderator at: 11/18/2011 10:58 AM |
|
12/12/2011 10:35 AM | |
Joined: 10/26/2011 Last visit: 4/22/2024 Posts: 760 Rating: (190) |
Hello Asdian, do you have also the problem on the second client, if you switch the licences form the first client to the second? If yes, than the missing licenses are the reason of your problem. Please check. Regards |
SIMATIC PCS 7 - Overview |
|
Follow us on