11/15/2005 10:09 AM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating: (150)
|
There is a Channel Development Kit (CDK) option to allow you to program your own drivers. Another alternative may be to use the third party product Omniserver. Omniserver is a communication driver that allows you to program in the protocol used to talk to your device. It can then use either DDE or OPC to pass the data to WinCC. http://www.omnidssi.com WinCC and DDE aren't very compatible with the current version (as you have already found) so I would suggest looking for suitable alternatives. Hopefully one of the above may be of use. |