5/23/2007 1:17 PM | |
Posts: 3149 Rating: (171)
|
Hi I searched WinCC help for modbus and you are right with WinCC V6 the modbus-driver is only available at allemendinger. nemo |
6/13/2007 2:38 PM | |
Posts: 54 Rating: (2) |
I' ve imported the drivers for modbus forom WinCC v5 to v6 and it is working. |
10/11/2008 7:31 AM | |
Posts: 8 Rating: (0) |
hai Darius, i have the same problem for WINCC and MODBUS, Can u pls sent me the Modbus driver for running in WinCC6.2. Thanks & Regards, Balu |
1/19/2009 1:42 PM | |
Posts: 1776 Rating: (95)
|
Hi, as mentioned in this FAQ http://support.automation.siemens.com/WW/view/en/21915573 you can order the modbus channel at www.allmendinger.de |
6/25/2009 11:51 AM | |
Posts: 2 Rating: (0) |
Does this mean that the only Siemens supported solution to interface with Modbus Slave is touse S7-300 or S7-400 with loadable driver on CP 341 or CP 441-2? |
Follow us on