2/19/2009 12:29 PM | |
Posts: 1275 Rating: (123)
|
Hi, What exactly are you trying to achieve? Do you want to input data on the WinCC database or collect data from it, to export to another system? Anyway... any access to WinCC's database by any third-party software requires an additional license. If you want to export online data you can do so through a script, and if you want to export data from a trend view you can also do this easily with no additional license. But to access the database (archives, such as TagLogging or AlarmLogging data) you'll need an option license. There are a few options for that, and you should try to find the one that better suits you. Some examples are: Connectivity Pack, which allows access from third party software to the database; DataMonitor, which allows for remote data visualization and IndustrialDataBridge, which allows for third-party software to access tags and archives. There are also add-ons, such as PM-OPEN EXPORT, but I don't know all that much about those. You can get some info on them through the links I've posted. I've also posted a little flowchart on data export which may help. You can also find a lot of information on this site, since data export has been discussed many times. Best regards, Danielle |
This contribution was helpful to1 thankful Users |
11/6/2009 7:26 AM | |
Posts: 325 Rating: (13) |
Hi New_Bird, U mean to say that u are unable to get back ur old alarms in the wincc?? U can try the Open selections dialogue. Regards Nil |
Follow us on