6/30/2013 3:13 PM | |
Posts: 3 Rating: (0) |
@ Amit_86 , @Pranav J. Bhagat Yes I know it can be done by text list or if only 2 texts then it can be by simple dynamization also. But I want to know the use of printf keyword in C-Action |
6/30/2013 7:45 PM | |
Posts: 3 Rating: (0) |
Thanks a lot. Great Suggestion. |
6/30/2013 10:32 PM | |
Posts: 62 Rating: (4) |
Dear Friend, There are standard Fonctions avb in the Wincc for Set & Get the Char Data . for reading the Char Data in the Object: GetPropChar(lpszPictureName,"EAFeld1","Tooltiptext"); in this Example :lpszPictureNamereturns the Parent Pictureor else u can give theother Picture name. EAFeld1: is Object Name Tooltiptext: Property for setting the Char Data inthe Object.: SetPropChar(LPCTSTR lpszPictureName, LPCTSTR lpszObjectName, LPCTSTR lpszPropertyName, char* szValue); I think this will resolve your Problem. Regards, Avinashkrishna Bhimavarapu. AttachmentScripts Help.zip (808 Downloads) |
Last edited by: Avinashkrishna at: 7/1/2013 8:17 AMLast edited by: Avinashkrishna at: 6/30/2013 11:58 PM |
|
This contribution was helpful to1 thankful Users |
7/1/2013 10:11 AM | |
Joined: 10/3/2010 Last visit: 9/19/2024 Posts: 1562 Rating: (191) |
please check "C for WinCC-course" as attached
AttachmentC For WinCC.pdf (1390 Downloads) |
B r g d s , |
|
This contribution was helpful to2 thankful Users |
Follow us on