10/8/2015 7:59 PM | |
Joined: 9/23/2005 Last visit: 9/17/2024 Posts: 4347 Rating: (1446)
|
“Simple Samples” are small projects that demonstrate simple features. The target is give a quick overview about the theme and be used as start point for related discussions. Follow there are a short description and the configuration main steps.
Description:
In this simple sample, two trends are displayed on HMI start screen by button click (the concept could be extended to controller commands).
The corn of the task solution is to build a control word where the most significant bit commands the trend “plotting” and the other word bits represents the trend curves to be plotted.
Requirements: WinCC Comfort V13 SP1.
Project with a minimum configuration (stop button, tags, etc. ).
Configuration main steps:
To update (plot a new point) of PLC_Tag_1 Place a button and configure on click event the follow functions:
To update (plot a new point) of PLC_Tag_2 Place a button and configure on click event the follow functions:
To update (plot a new point) of PLC_Tag_1 and PLC_Tag_2 Place a button and configure on click event the follow functions:
References: Manual WinCC Professional V13.0 https://support.industry.siemens.com/cs/br/pt/view/92323076/en
Online helps system WinCC Professional V13.0 SP1 https://support.industry.siemens.com/cs/br/pt/view/109096785/en
Application and tools Demo projects for HMI operator panels under WinCC V13 (TIA Portal) for Basic Panels (2nd generation) and Comfort Panels https://support.industry.siemens.com/cs/br/pt/view/96003274/en
FAQ Which VBS information and VBS programming tools are there in WinCC (TIA Portal)? https://support.industry.siemens.com/cs/br/pt/view/59885894/en
Tips and tricks for creating scripts in WinCC (TIA Portal) https://support.industry.siemens.com/cs/br/pt/view/57132412/en
Project: Attached as project.zip.
AttachmentProject.zip (486 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to4 thankful Users |
Follow us on