2/4/2017 1:57 PM | |
Joined: 9/23/2005 Last visit: 5/21/2024 Posts: 4326 Rating: (1426)
|
“Simple Samples” are small projects that demonstrate simple features. The target is give a quick overview about the theme and be used as start point for related discussions. Follow there are a short description and the configuration main steps. Description: In this sample, a controller's user program Program_alarm block call will generate a message on a HMI. The instance DB name will be part of the alarm text. Alarm messages are an important tool for operation diagnose of process and system events. Adding the instance DB name as part of the alarm text, it is possible to individualize any block call message. The possibility to generate messages directly from the controller's blocks reduces the HMI configuration time. The same main steps are also applicable to WinCC Advanced / WinCC Professional. Requirements: WinCC Comfort V14. Configuration main steps: On Controller side:
On HMI side:
TIP:it is possible to use other blocks (GetSymbleName, GetSymblePath, GetInstancePath, GetBlockName) instead of GetInstanceName to add information to the messages. References: /1/WinCC Advanced V13 SP1 – Simple Sample: Invert Bit Program_alarm block Help system (F1) GetSimbolicName block Help system (F1) Project: Archived program, compressed (zip) AttachmentProject2.zip (878 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to1 thankful Users |
5/31/2020 7:20 PM | |
Posts: 18 Rating: (3) |
Is the "Program_Alarm" block only available on the S7-1500 series of controllers, I cannot find it on my instruction list for my Sy-1200? |
6/9/2020 9:56 PM | |
Posts: 18 Rating: (3) |
That answes that one - Thank you 👍 |
3/17/2021 9:48 AM | |
Posts: 8 Rating: (0) |
Hi , you cannot use "Program_Alarm" in S71500 and BasicPanel? Bye MartinIT |
Follow us on