9/15/2010 10:14 AM | |
Posts: 3 Rating: (0) |
Hi All, I have installed WinCC ver 7.0 SP1 HF5 and Step 7 v5.4 SP5 HF1 on my laptop.The OS on my machine is Windows XP SP3. I am getting the following error when I try to run Step 7 "The project contains objects of the software package 'WinCC(Component Object Manager)' which can not be edited because the software package is not installed or exists in an earlier version." see attached screenshot. There has been no previous installation of Wincc or Step 7 on the laptop before. Attachmentwincc_component_mgr_error.pdf (895 Downloads) |
This contribution was helpful to1 thankful Users |
9/15/2010 7:55 PM | |
Posts: 510 Rating: (117) |
The component you are missing is installed with WinCC. You have to select the user defined installation to find the component you require. More details can be found in this thread: /tf/WW/en/Posts/44879 |
9/16/2010 9:07 AM | |
Posts: 3 Rating: (0) |
Thanks Bill, let me try that and I will let you know how it goes. |
Follow us on