3/13/2008 8:50 AM | |
Posts: 1776 Rating: (95)
|
Hi, what do you mean with connection configuration tool??? Do you mean communication configurator?? |
3/17/2008 2:39 PM | |
Posts: 1776 Rating: (95)
|
Hi, maybe the communication drives is not installed. See WinCC Online help Smart tools > WinCC configuration tool > Diagnostics > Error column |
6/6/2012 12:36 PM | |
Joined: 5/20/2011 Last visit: 4/18/2024 Posts: 5 Rating: (0) |
I have the same problem. The above transaction yields no solution at all. Please advise. |
12/8/2013 5:28 PM | |
Posts: 5 Rating: (0) |
The same problem happend to me, I could not find any solution for that. The system config: Windows7 Pro 64bit WinCC 7.0 SP3 Office 2007 (I have tried Office 2003 as well) Clean windows installation. With Excel configuration tool, I'am trying to connect to an existing project. The first message is "Not all limit monitorin ...". When I check the Reading Error tab, The message is as below: Type : Error Table type : Connection table Error text : The communication driver set is unknown! I would be appriciated for any advise. Regards |