10/12/2015 2:00 PM | |
Posts: 63 Rating: (1) |
Attached is the log file, I thick . Every connection has errorCode = 0x8000152100000084? In Set PG/PC Interface there are three Interface Parameter Assignments: …with ISO protocol, …with TCP/IP protocol and ... assignment for the IE-PG access…. . Which one should I choose? I have tried switching between them. AttachmentLog_file.zip (125 Downloads) |
10/12/2015 4:17 PM | |
Posts: 63 Rating: (1) |
Hi Georg. I don’t have a file called Simatic S7ProtocolSuit.log. Att.1 is a pic of the diagnose folder. As is then I am using a two separate PCs, one for TIA PORTAL programming and one for the WinCC RT which is connected to the PLCs. In the Prg. PC I can only select network adapters that are in that PC not the ones that is in the WinCC PC. See Att.2). Regards Ari AttachmentAtt1_2.zip (186 Downloads) |
Follow us on