Industry Online Support
Technical Forum
3/5/2010 6:08 PM | |
Posts: 12 Rating: (4) |
Thanks for the reply Actually my situation here, I have 2 client which have identical application. In one client when I call the Date function in VB I am getting the Format according to the Regional setting which is working fine. But in another Client when I call the Date function in VB it is not accoridng to the Regional setting. Let me know what can be the problem?? The Client Date function which is not matching the regional setting, it is recently formatted & installed windows with all required WINCC packages. Regards Prem kumar |
3/6/2010 3:04 PM | |
Posts: 39 Rating: (3) |
Hi, This usually happens when u generate reports from the Archive. The Archive of WinCC program are stored in SQL Server. And, the default time of SQL is set to UTC not to regional time. For example: when you look at the alarm at runtime, you will get the correct time stamp which is the same as ur regional time (bcz WinCC automatically converts the time for you). However, if you open the sql database and look at the alarm archive, you will see the time is different. To make sure you don't have this problem, google on how to set SQL time to regional time. Good luck. |
4/9/2010 9:03 AM | |
Posts: 12 Rating: (4) |
Hi, Still I am not able to Fix this Bug..... |
8/13/2010 1:11 PM | |
Joined: 8/13/2010 Last visit: 9/16/2024 Posts: 2 Rating: (0) |
I have the same problem with the trending in WinCC V6. Client1 trough 4 gives in the trending the format: dd/MM/yyyy Client5 gives in the trending the format: MM/dd/yyyy Client 2 trough 5 are ref. clients so the WinCC settings are identical. The regional setting are also the same on all the clients... |
8/18/2010 12:31 PM | |
Joined: 1/4/2010 Last visit: 9/13/2024 Posts: 650 Rating: (40)
|
Hi You change also the"Date" tab? http://support.automation.siemens.com/WW/view/en/11377522 |
Regards |
|
Follow us on