Industry Online Support
Technical Forum
6/18/2010 8:22 AM | |
Joined: 2/6/2009 Last visit: 3/21/2024 Posts: 938 Rating: (118) |
DearS.S.D.D., I am using S7 313c and TP177B and I am able to communicate between PLC Sim and Flexible Runtime through MPI. All you need to do is, *Download your PLC program to the Simulater. ( SetPG/PC will automatically changes to PC Adapter TCP/IP). *Open WinCC Flexible backup and select Flexible Runtime, You should not select Flexible simulator. I am using the same method and it is working fine. Revert Back for any clarification.
|
_______________________________________________________________ |
|
6/18/2010 1:54 PM | |
Posts: 67 Rating: (0) |
Thanks for the help. I was using the simulator like I normally do just to test out picture functions, not the runtime! |
Follow us on