Industry Online Support
Technical Forum
12/17/2012 11:35 AM | |
Posts: 101 Rating: (6) |
Hello, First of all, I'll list what software/hardware I'm using:
I can ping the PC, and I can ping my laptop, so the networking is OK. I have the RT Loader program open and in transfer mode. The problem is this: When I add the device in a TIA project I cannot go online. When I try to load a program to the PC it gives me this error: "The required operating system is not installed on the HMI device. Update the operating system from WinCC with the menu command "Online > HMI device maintenance > Update operating system"." I cannot do the action described in the error because I cannot go online. I've attached a TIA project so you can see the hardware config. Any help or demo projects would be appreciated very much. Thanks, Jeremy
AttachmentWinCC Test.zip (241 Downloads) |
Follow us on