5/26/2009 9:26 AM | |
Joined: 5/8/2006 Last visit: 4/29/2024 Posts: 1085 Rating: (77) |
Hi I think you should create an Support Request at Siemens. If you need an short-term solution, you can modify the graphic in MS Paint. Bye |
5/26/2009 2:56 PM | |
Posts: 16 Rating: (1) |
I made a notify to Siemens, will see what's going to happen now? There's a link to our discussion. |
5/27/2009 9:33 AM | |
Posts: 12 Rating: (0) |
Darius, The original image is one of my digital photographs that was re-sized and converted using Gimp 2. The attached zip file contains the 3 images displayed in the previous posting so you can try it for yourself. The choice of panel may have a bearing on how the pictures are displayed, I selected MP370 12" touch but I'd be interested to know if results differ from one panel to another. I also found it interesting that the PNG file is twice the size of the GIF but doesn't display so well. Nick AttachmentP2050933-01-1280.zip (193 Downloads) |
6/16/2009 9:48 AM | |
Joined: 4/24/2006 Last visit: 9/25/2024 Posts: 8742 Rating: (1168) |
Dear heguli, Perhaps Hotfix 1 for WinCC flexible 2008 + sp1, might help. http://support.automation.siemens.com/WW/view/en/36540041 Best regards, Wizard |
Follow us on