12/16/2011 1:19 PM | |
Posts: 3037 Rating: (192)
|
Hello, Do you use a PC or a Panel for your project? Do you exit the Runtime with the function"StopRutime"? Tweety |
12/16/2011 1:48 PM | |
Posts: 50 Rating: (0) |
If I have the runtime on a PC, perform tests on the Exit button on the file runtime but equally restarts from 0 to delete the data you had before, thanks. |
12/16/2011 3:40 PM | |
Posts: 3037 Rating: (192)
|
Hello, I can not understand you. What do you do exactly? (Step by Step) Do you have a panel or PC? Do you use data log or alarm log? You need information for logging, see the following FAQ: How are tags and alarms logged in WinCC flexible? Tweety |
12/20/2011 2:22 AM | |
Posts: 50 Rating: (0) |
if I use the stop function runtime, I have thought of doing as you said with a script I am using the scheduler function to run a script every 1 minute, place the script file function to stop and then I put the copy function file but it says error copying file in C: / Logs, thanks for your help!
AttachmentDibujo.pdf (73 Downloads) |
Follow us on