5/28/2010 1:19 PM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181)
|
Hello, Look atWhat transfer options are available in the various operator panels? There you'll find what kind of cable is need, deppends of P = Process coupling K = Optional process coupling D = Download (update operating system, project, …) U = Booting (filling in the case of a missing or damaged operating system) Best regards, Hristo Mihalev |
Last edited by: UMENCHO at: 5/28/2010 1:20 PM |
|
This contribution was helpful to1 thankful Users |
5/28/2010 2:30 PM | |
Joined: 1/17/2007 Last visit: 10/6/2020 Posts: 289 Rating: (3) |
Thanks again. Looks that for OP77B this adapter isn't working. |
5/28/2010 2:38 PM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181)
|
Best regards, Hristo Mihalev |
6/28/2010 10:18 AM | |
Joined: 1/17/2007 Last visit: 10/6/2020 Posts: 289 Rating: (3) |
Where to find a procedure for project download to OP77A using PC ADAPTER 6ES7972-0CB20-0XA0 ? Thank you. |
6/28/2010 10:39 AM | |
Joined: 5/28/2008 Last visit: 9/9/2024 Posts: 4515 Rating: (839) |
Hello ionut.b, As Umecho said that USB PC adapter is not realeased for transfer. Please see note 6 in Umencho's Link "What transfer options are available in the various operator panels?" You can transfer to the OP77B using MPI protocol via MPI cable connected between PG and the panel but not via USB PC adapter. Hope this helps. |
Ayman Elotaify |
|
6/29/2010 11:12 AM | |
Joined: 1/17/2007 Last visit: 10/6/2020 Posts: 289 Rating: (3) |
Yes, this option is also enabled. I will try to use an USB/PPI adapter to see if it works. Thanks. |
Follow us on