5/9/2014 4:11 PM | |
Posts: 133 Rating: (0) |
how it could be ?, no scripts |
5/9/2014 4:15 PM | |
Posts: 133 Rating: (0) |
i found it, help me |
5/9/2014 4:18 PM | |
Joined: 4/24/2006 Last visit: 4/26/2024 Posts: 8616 Rating: (1147)
|
Hi, Delete it when you do not want to use it Best regards, Wizard |
5/9/2014 4:47 PM | |
Posts: 133 Rating: (0) |
i deleted it and compiled, this time it is said: attemp to refer to an undefined script (perhaps deleted) |
5/12/2014 6:44 PM | |
Posts: 133 Rating: (0) |
dear vipz, no it is not done!! dearAyman Elotaify, I tried that but the error message remai-ns the same.
|
5/12/2014 6:52 PM | |
Joined: 5/28/2008 Last visit: 4/15/2024 Posts: 4505 Rating: (835) |
Helloallayahassine, You have told that you created a simple project and you could run it without problems using RT software. This means that there's no problem in the WinCC flexible installation. I just wanted to confirm that you did this step on the same computer. Please confirm In this case, it's clear for all of us that the problem is in the project itself. So, I do not think that anybody can investigate or guess where's the problem without seeing the software. You can contact your local Siemens representative for help or sending the software to technical support using support request tab in the right hand side navigator of this site. Hope this helps.
|
Ayman Elotaify |
|
5/12/2014 6:59 PM | |
Posts: 133 Rating: (0) |
Yes i confirm that the dummy project which runned succesfully is on the same computer as the original project (not able to running), thank you |
Follow us on