4/24/2016 6:57 AM | |
Joined: 11/21/2007 Last visit: 8/12/2024 Posts: 2325 Rating: (308) |
WinCC Flexible 2008 SP2 is not compatible with Windows7 64 bit. AttachmentWinCC-flexible_2008_compatibility-list_en_2016-04-20.xlsx (358 Downloads) |
There is no such thing as the last bug in a program |
|
4/24/2016 7:22 AM | |
Joined: 10/2/2013 Last visit: 9/22/2024 Posts: 339 Rating: (52) |
There are many reasons for slow work, Have you try start as administrator ? You should check yor RAM under use with use of task manager, when you start project. Check your system compatibility with use of below Link http://www.siemens.com/kompatool What ever your conclusion please explain here.. |
Technology is best when it brings people together,so we are here now :) |
|
4/24/2016 9:46 AM | |
Joined: 9/22/2014 Last visit: 6/12/2024 Posts: 89 Rating: (13) |
Hello , Try removing all the temp files and catche files from your computer. Also clear recycle bin. Pratts23 |
4/24/2016 10:38 AM | |
Joined: 5/28/2008 Last visit: 9/21/2024 Posts: 4515 Rating: (839) |
Hello Saeedplc, From day one of release of WinCC flexible SP3, Siemens encountered problems with HP laptops! But the problem as far as I know was limited to the driver of the keyboard. Please have a look here: What should you watch out for when installing WinCC flexible 2008 SP3 or WinCC V11 SP2 on an HP notebook?I am not sure that this problem solved in later updates or not because there is no official statement from Siemens to tell that the problem solved. But in any case you can try to download the latest update from the following link and tell us if it solved your problem or not. Update for WinCC flexible 2008 Service Pack 3 |
Ayman Elotaify |
|
This contribution was helpful to3 thankful Users |
4/24/2016 11:33 AM | |
Joined: 7/22/2008 Last visit: 4/14/2022 Posts: 1884 Rating: (174) |
RIP |
Last edited by: 1test at: 6/8/2016 9:32:40 AM~(‾▿‾)~ |
|
4/24/2016 11:51 AM | |
Joined: 7/22/2008 Last visit: 4/14/2022 Posts: 1884 Rating: (174) |
RIP |
Last edited by: 1test at: 6/8/2016 9:32:53 AM~(‾▿‾)~ |
|
This contribution was helpful to2 thankful Users |
Follow us on