4/26/2013 10:05 AM | |
Posts: 33 Rating: (1) |
Hi Is there a way to acknowledge only horn (sound part) in wincc when alarm comes? What happens is that alarm comes, and horn (sound alarm) activates. Then i acknowlage the alarm with the button and the sound from horn is gone but also alarm disappears, because the acknowledgement has set signal tag. What i want to do is that when alarm comes is to acknowledge this alarm, and that the sound from horn is disabled but i want to leave this alarm in the alarm list, but without the sound once it is confirmed.
AttachmentDesktop.zip (310 Downloads) |
4/30/2013 9:32 AM | |
Posts: 1530 Rating: (59)
|
Hello Pero51, please take a look at this: WinCC horn when a message arrives How can you signal messages acoustically? How is the horn editor configured for single-user stations, servers, redundant servers and client OS stations in SIMATIC PCS 7 / WinCC? Best regards Bizur |
This contribution was helpful to1 thankful Users |
12/29/2013 12:59 PM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2683 Rating: (135) |
New question splitted to alarm should not dis-apperar from the alarm bar,untill the fault has resolved Best regards O_Moderator |
Follow us on