Industry Online Support
Technical Forum
6/1/2008 7:47 AM | |
Joined: 9/7/2007 Last visit: 8/30/2023 Posts: 550 Rating: (61) |
Hi Nithin, there are somethings I would like to check if you adjust it during installation or not. first I would like to check if you adjusted the local security policy or not. If not please check the attached file. Moreover it is preferred to turn the firewall of till the installation end. Last I recommend to reinstall a fresh Windows XP again and try sometimes errors occurs during Installation AttachmentWinCC V6.2 Installation Notes 2006.pdf (60 Downloads) |
Best Regards |
|
6/20/2008 2:57 PM | |
Posts: 48 Rating: (0) |
Hello sir , thanks. But the problem was another thing. I hadn't the LAN driver installed. As soon as i Installed it the problem got away. |
Follow us on