Industry Online Support
Technical Forum
7/6/2010 7:54 AM | |
Posts: 108 Rating: (4) |
I don't know how you can set password for WinCC CS, but you will try to unistall WinCC CS-then no body could not have a rights for editing project. |
7/7/2010 9:37 AM | |
Posts: 133 Rating: (0) |
so the only sollution is to instal the runtime ??? are you sure a can`t protect WinccExplorer with a password ?? Regards, |
7/7/2010 10:59 AM | |
Joined: 1/4/2010 Last visit: 9/13/2024 Posts: 650 Rating: (40)
|
Hi You can lock the key have a look in the FAQs, so you can't change from WinCCto the WinCC Explorer. http://support.automation.siemens.com/WW/view/en/27068495 http://support.automation.siemens.com/WW/view/en/22326881 In WinCC Runtime you have a button for exit Runtime. For this button you have to change the authorization sothat not all user can push this button. |
Regards |
|
7/8/2010 7:57 AM | |
Posts: 133 Rating: (0) |
unfortunately link that you provide doesn`t help to secure my wincc project. scada window is not full screen . can i password WinccExplorer ? and also disable WinccDuplicator ? only solution is to instal only the runtime version Wincc V7.0 SP1 . Regards |
7/8/2010 8:13 AM | |
Posts: 133 Rating: (0) |
hei , nobody knows how to protect the copyright of a project WinCC. ?! I understand thar in runtime version , WinCC explorer is active 1 hour ? |
Follow us on