1/22/2013 4:35 PM | |
Posts: 8 Rating: (0) |
hey Yolov, thank you so much, excellent answer i will check and see if i need more help from you |
1/24/2013 10:11 PM | |
Posts: 8 Rating: (0) |
Mr. Yolov, please let me know ifadifferentUSB smart card reader/writercan be used instead of the SIEMENS? |
1/25/2013 9:25 AM | |
Joined: 2/22/2006 Last visit: 3/29/2024 Posts: 290 Rating: (37) |
Hi, Yes you are right, 6ES7 652-0XX05-1XD1 is considered phase-out product. There is new product: SIMATIC PCS 7 TCOS 3.0 CHIPCARD FOR CHIPCARD READER; 10 PIECES PER PACKAGING UNIT; PLEASE NOTE THE PCS 7 SOFTWARE COMPATIBILITY; SEE PRODIS ENTRY-ID. 29700431 and the chpcard reader is: SIMATIC PCS7, USB CHIP CARD READER, DESK-TOP CHIP CARD READER, INCL. USB CONNECTING CABLE, AS OF PCS7 V6.1 + SP1/ WINCC V6.0 + SP3A AND ONLY IN CONNECTION WITH SIMATIC LOGON AS OF VERSION 1.4 SP1 OR HIGHER RELEASED As you can see it is comparible with SIMATIC LOGON v1.4 SP1 upwords. The biometric mouse is quite expensive - more than 8000 EUR. But it is up to you to decide which product you will use. In may last project I used USB acrd reader bought by Siemens. It is OMNYKEY 3121 (more information here: http://www.hidglobal.com/products/readers/omnikey/3121). Probably you can use another chipcard readers, if their drivers are supported by SIMATIC LOGON. Info for biometric mouse you can find in SIMATICPCS7_STPCS72_complete_English_2010-09.pdf catalog, page 5/20. For you convenience it is attached. it is not the last one (just I could not find the lat one). Good luck, Svetozar Yolov AttachmentSIMATICPCS7_STPCS72_complete_English_2010-09.pdf (294 Downloads) |
This contribution was helpful to1 thankful Users |
1/25/2013 11:18 AM | |
Posts: 1530 Rating: (59)
|
Hello ManriqueMurillo, seems like all your questions will be solved with great help of user "Yolov". So, this thread can be closed. Best regards Bizur |
Follow us on