1/12/2011 7:09 AM | |
Joined: 4/14/2010 Last visit: 4/3/2024 Posts: 525 Rating: (11) |
Hello Can every body help me how can i Migrate the wincc project file into wincc flexible (see attached) Which software required to open the mcp. project file.???? Thanks. Attachmentmcp.zip (52 Downloads) |
MS |
|
1/12/2011 7:37 AM | |
Joined: 3/21/2006 Last visit: 4/4/2024 Posts: 10228 Rating: (1181) |
Hello Muhammad Sarfraz, Take a look at one old discussion here concerning WinCC migration - Wincc 6.2 SP2 to Winccflex 2007 HF4 Mi gration . You don't need any extra software. "Migration" is supplied with WinCC flexible. WinCC flexible setup automatically installs it on the engineering station if you selected the "standard" setup. You can install the program either immediately or at any other time if you select the "userdefined" setup of WinCC flexible. But also the final result is not perfect. Best regards, Hristo Mihalev |
Follow us on