8/12/2013 2:39 PM | |
Joined: 11/21/2007 Last visit: 8/12/2024 Posts: 2325 Rating: (308) |
Hi I am trying to install SP2 for WInCC V11 from the Link Service Pack 2 for WinCC V11 All the Downloads consist of several files of 650MB which are later merged together to form the Indtall. However If I try to download the WinCC V11 Professional SP2, the filw sizes ( When downloaded ) are not 650MB ( e.g. .001 file is 340MB ). So when I try to run the Exe file to merge all the files, I get a Error Msg. There is no such problem with WinCC Basic / Advanced. Can someone pl help me in this. Thanks Navnag |
There is no such thing as the last bug in a program |
|
8/13/2013 12:45 PM | |
Joined: 11/21/2007 Last visit: 8/12/2024 Posts: 2325 Rating: (308) |
Thanks Pegaia I have tried Downloading from Chrome ( Was using IE earlier ). Also tried from 2 other PCs .. Same result I am getting the following sizes always :( Pl see attachment ) No such problem with WinCC Basic SP2 Regards Navnag |
There is no such thing as the last bug in a program |
|
8/14/2013 9:17 AM | |
Joined: 9/1/2005 Last visit: 9/18/2024 Posts: 4104 Rating: (195) |
Hello Navnag, please try again to download. You could use the browser your want to use It should work now. Some background information: For a longer periode this Servicpack wasn't downloaded. So it wasn't cashed anymore. With your request only a short version was available. But now it should be the whole package again. Thank you for asking publishing this question. Our colleague trying to check why it happens so that this behavior could be fixed. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
This contribution was helpful to1 thankful Users |
8/14/2013 8:24 PM | |
Joined: 11/21/2007 Last visit: 8/12/2024 Posts: 2325 Rating: (308) |
HI CS Moderator Thanks a Ton. I have now been able to download all the files and they are showing the correct sizes We have also been able to install the downloaded files without any problem. Cheers Navnag |
Last edited by: Navnag at: 8/21/2013 5:46 AMSuccessful Install Comment added There is no such thing as the last bug in a program |
|
This contribution was helpful to1 thankful Users |
Follow us on