8/24/2016 2:41 PM | |
Joined: 12/13/2011 Last visit: 4/19/2023 Posts: 123 Rating: (12) |
WinCC Professional Runtime V13 SP1 Update 9: Hello, Is there a function in WinCC Professional to stop the Graphics Runtime only(other than from the System Tray)? I want to keep the WinCC services such as the OPC Server running and be able to close the graphics. Thanks, masmith1553 ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 8/24/2016 4:00:56 PMNew subject after splitting |
|
8/24/2016 3:23 PM | |
Joined: 12/13/2011 Last visit: 4/19/2023 Posts: 123 Rating: (12) |
Ok, I did some research and found out how to solve my problem. I found this forum with the code below for the solution:
It worked like I wanted. Thanks, masmith1553 |
This contribution was helpful to1 thankful Users |
8/24/2016 4:05 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4777 Rating: (123) |
The second thread with the subject WinCC Pro V13 SP1 Update 9: Stop Graphics Runtime from Runtime is published within the conference SIMATIC WinCC /TIA Portal). Best regards |
Follow us on