1/7/2014 10:33 AM | |
Posts: 1299 Rating: (136)
|
Hello, i just testedthis and it works... can you please add some screenshots of your project? did you try to change the layer of the button? K!ke |
1/7/2014 10:46 AM | |
Posts: 101 Rating: (7) |
Oh, I asked support and forgot to post it here. I explained this slightly wrong. If you have a faceplate with invisible elements in it, then objects under it are not clickable in Professional. They are in clickable in Advanced. Support says this is normal. Sample project attached. Answer from support: we tested now every single possibility: - faceplate (with visible objects in it) over a button -faceplate (with invisible objects in it) over a button => you are not able to click the button in bothexamplesbut that wasn't ever possible in WinCC Professional. Not in WinCC V7.2 and not in WinCC Professional V12. There is no hierarchy between the objects. The functions which are working in Advance don't have to work in Professionalbecause these are developed intwo different development services.
AttachmentTestProjectInvisibleFaceplate.zip (251 Downloads) |
Last edited by: Jeremy Mahieu at: 1/7/2014 10:47 AM |
|
Follow us on