7/13/2012 12:17 PM | |
Posts: 6 Rating: (0) |
Compile -> All |
7/13/2012 4:45 PM | |
Posts: 3037 Rating: (192)
|
Hello, You can delete the folder "IM" in your project directory. If you compile the project new, this folder is generated newly. You should use this update for Runtime Professional Updates for WinCC Runtime Professional V11 SP2 Do you have the problems only since update 3? Tweety |
7/18/2012 10:47 AM | |
Posts: 3037 Rating: (192)
|
Hello, What did you modify in your project? You should test the download with a new project. Does the error appear still? Tweety |
7/18/2012 11:05 AM | |
Posts: 6 Rating: (0) |
I can download the project to the HMI PC station with file transfer without problems. These errors appear only when I click "Go Online" button. Regards, Tõnis |
7/18/2012 4:41 PM | |
Posts: 3037 Rating: (192)
|
Hello, Do you use the right settings in the PC/PG interface on this PC? Do you use the right access point at your connection of plc? Tweety |
7/18/2012 7:21 PM | |
Posts: 6 Rating: (0) |
Attached image of PG/PC interface. |
7/19/2012 12:41 PM | |
Posts: 3037 Rating: (192)
|
And your access point in the connection of plc? Does the access point call "S7ONLINE"? See the screenshot. Tweety |
Follow us on