10/13/2008 7:44 AM | |
Posts: 8 Rating: (0) |
dear all, Recently I met a problem on PCS7 server redundancy. I use twoHP DL580 G4 servers for WinCC redundancy, but when next systemrestart it always pop errors, which say "Wincc redundancy controlmodule encountered a problem and needed to be close". Once the error was thrown out, the client cannot connect this server and cannot switch to thegood server. Why? I have reinstalled windows server 2k3 and pcs7 serveral times, but nothing changed. System environment: Servers: Windows Server 2003 standard +sp1 Client: Windows XP+sp2 PCS7 version: v6.1+sp1 the attachment is software installed in servers and the error dialog box. thanks! Attachmenterror_img.zip (240 Downloads) |
Last edited by: FleXoluTion2008 at: 10/13/2008 7:50 AM |
|
10/15/2008 11:55 PM | |
Posts: 2661 Rating: (279) |
Hi TIC, I am sure PCS7 V6.1 SP2 is supported. See following link: New SIMATIC PCS 7 Industrial Workstations Type 547B with SIMATIC PCS 7 V6.1 + SP2 Released for Delivery |