8/16/2013 9:13 AM | |
Joined: 4/24/2006 Last visit: 9/18/2024 Posts: 8738 Rating: (1168)
|
Hello Berg, Perhaps this link might help: Which settings must you make on the RT Loader to transfer a WinCC flexible Runtime file from the configuration computer to a visualization PC? Best regards, Wizard |
This contribution was helpful to2 thankful Users |
8/16/2013 8:07 PM | |
Joined: 1/17/2006 Last visit: 8/18/2024 Posts: 553 Rating: (29) |
Thanks for the info. I will try it ! regards.
|
"Educate the children and it won't be necessary to punish the men." |
|
8/20/2013 4:10 AM | |
Joined: 1/17/2006 Last visit: 8/18/2024 Posts: 553 Rating: (29) |
Hi. Unsuccessfully. I cannot make the transfer of my Laptop (WinCC flexible 2008 SP3) to IPC277D via Ethernet. An attempt is made to transfer but the message "Check your settings, interface, cables etc.." is shown. Using ping command it's possible to find the IPC (192.168.0.2) without problems and also if I copy the application with USB application communicatesseamlessly with the S7-300. The problem I can't make the transfer via Ethernet directly. It's boring pass via pendrive the changes all the time ... Best regards. |
"Educate the children and it won't be necessary to punish the men." |
|
8/20/2013 4:48 PM | |
Joined: 4/24/2006 Last visit: 9/18/2024 Posts: 8738 Rating: (1168)
|
Hello Berg, Is the visualization PC (IPC277D) in transfer mode? Best regards, Wizard |
8/21/2013 11:04 AM | |
Posts: 3037 Rating: (192)
|
Hello, Can you see your IPC under STEP 7 > PLC > Edit Ethernet Node... > Nodes accessible online. Tweety |
Follow us on