4/19/2016 10:49 AM | |
Joined: 6/3/2014 Last visit: 1/17/2023 Posts: 660 Rating: (191) |
Hello Gotare, as the error message points out the proxy device it wold be helpful to get some more information here. Did you use the proxy device earlier or for this project? Maybe there is a rest of a connection that hasn't be deleted. Did you install SP1? In V13 SP1 the proxy device should be in the hardware catalog under "Controllers". Did you create a new project or upgrade an old one? / Do you get the same error if you start a new clean project? You could try installing the proxy device GSD file, but that is only for direct buttons on a panel, normally. Here is the application example for proxy device, if you're interested: https://support.industry.siemens.com/cs/ww/de/view/73502293 |
~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
This contribution was helpful to1 thankful Users |
4/9/2020 5:08 PM | |
Joined: 5/11/2015 Last visit: 9/18/2023 Posts: 1 Rating: (0) |
Same Issue i am facing .i even reinstalled the software but wincc RT ,HMI screen still appear anyone please |
Follow us on