5/10/2012 10:00 AM | |
Posts: 6 Rating: (0) |
Hi tavinho If you have can you please tell me how did you solve this problem because I'm expiriencing the same problem........ |
5/10/2012 10:19 AM | |
Joined: 10/3/2010 Last visit: 5/8/2024 Posts: 1552 Rating: (188) |
Please be more specific. What symptoms do you see/experience? Do you have screenshots to attach? Which version? ... Brgds. |
B r g d s , |
|
5/10/2012 3:37 PM | |
Posts: 6 Rating: (0) |
Hi I copied a project that was created on WinCC v6.2 SP2 on a windows 2003 machine (PC1) to another windows 2003 machine with the same version of WinCC (PC2). Changed the IP adress and the computer name of PC2 to be exactley the same as PC1, shut down and disconnected PC1.When I go to runtime on PC2 WinCC shows that it is not active (please refer to the attached) and the communication drive shows that it is DISCONNECTED. What could cause this problem? please help i'm a new user of this software........... Another thing how long can you run this softwareon demo? AttachmentNew Compressed (zipped) Folder.zip (159 Downloads) |
5/15/2012 4:56 PM | |
Posts: 6 Rating: (0) |
Hi Can someone who can help me please help....... I checked the channel diagnosis and saw that the Simatic S7 protocol suit with all the plc's connectedto itare not connected but when I ping the ip adress of the plc's it does show that it is connected to this station(PC2).Please refer to the attached....... Attachmentchannels and diagnosis.zip (137 Downloads) |
5/15/2012 9:40 PM | |
Joined: 10/3/2010 Last visit: 5/8/2024 Posts: 1552 Rating: (188) |
First try to check the diagnose folder and especially the file C:\Siemens\WinCC\Diagnose \SIMATIC_S7_Protocol_Suite_01.LOG Perhaps you can post the most recent content of it too? Brgds |
B r g d s , |
|
5/16/2012 12:54 PM | |
Posts: 6 Rating: (0) |
Hi SteBo Thank you for your reply.Here is the last content of the SIMATICS7 Protocol Suite log; refer to the attached...... Attachmentdiagnose.zip (149 Downloads) |
5/16/2012 1:45 PM | |
Joined: 10/3/2010 Last visit: 5/8/2024 Posts: 1552 Rating: (188) |
in that logfile, you have Error Code "0xFFDF 42C2":
you can find info about all error codes in the file "C:\Program Files\Siemens\WinCC\bin\S7CHNERRORENU.HLP" These are the first things to check but "Setting the PG/PC Interface" is the most forgotten cause. old thread that might help too Brgds. |
Last edited by: SteBo at: 5/16/2012 2:02 PMadded link Last edited by: SteBo at: 5/16/2012 1:48 PMB r g d s , |
|
This contribution was helpful to1 thankful Users |
Follow us on