11/23/2017 9:23 AM | |
Joined: 12/4/2009 Last visit: 5/3/2024 Posts: 452 Rating: (134) |
Dear experts, my system contains S7-1500 and WinCC RT Professional. TIA Portal version is V14 SP1 Update 2. WinCC RT Pro is configured for multiple monitors, following the guideline given in the FAQ entry: How do you use multiple monitors simultaneously with the WinCC (TIA Portal) Runtime Professional I also have a toolbar with one button configured to call login dialog popup window. So, as far as I can see, when I start runtime WinCC creates three separate threads in the taskbar: 1. Generic blank WinCC window; 2. Screen window for screen 1; 3. Screen window for screen 2. The problem arises when I click on the toolbar button to call login dialog. In that case WinCC puts focus on the blank screen (Generic WinCC blank window) and displays login popup window. Now, if I input correct username and password WinCC automatically restores screen windows for screen 1 and screen 2. But, if I input wrong credentials, WinCC informs me about unknown username/password and focus remains on the blank screen. The only way to restore my screen windows is to use Alt+Tab. But, if keyboard shortcuts are disabled, I am stuck on the blank screen. Any ideas how to overcome this annoying issue? Thanks in advance. Regards. |
Last edited by: crazyCow at: 11/23/2017 9:24:24 AMLast edited by: Jen_Moderator at: 7/9/2018 2:28:02 PMOptimized link. If this post actually helped, you may consider using the Rate button above. |
|
7/9/2018 11:44 AM | |
Joined: 1/5/2013 Last visit: 5/5/2024 Posts: 275 Rating: (16) |
old one, but i'm facing the same problem. any suggestions please? thanks |
Follow us on