8/23/2016 9:12 AM | |
Joined: 8/21/2016 Last visit: 7/12/2022 Posts: 20 Rating: (0) |
Hi, I'm trying to establish a connection between a Siemens PLC 1500 and my laptop. I need to use WinCC Professional for my application, but the problem is that the PC Station is not reachable. I set my PG-PC Interface, I connected WinCC to PLC through HMI connection and the PLC to PC Station through IE connection. The IPs are in the same class.. AttachmentPoze.zip (117 Downloads) |
8/23/2016 9:42 AM | |
Joined: 5/12/2006 Last visit: 4/23/2024 Posts: 22222 Rating: (2979)
|
Hello, do you use the WinCC RT Professional on the Laptop or the Simulation from the TIA Portal? Christoph |
Follow us on