(0)| 9/20/2021 1:15 PM | |
|
Joined: 2/5/2013 Last visit: 12/22/2025 Posts: 330 Rating:
|
Hi all, We are using below software and hardware in our project. 1.WinCC 7.5 SP1 Runtime 2.IM151-8 PN-DP (10 nos connection) on profinet. 3.CP1623 with hardnet license. 4. Windows 10 PC. The problem is when I start WinCC Runtime then 6 connection shows connection establishement with PLC.4 connection shows not connected Status to make the remaining one healthy I need to power off and Power on all CPUs and Start WinCC SCADA again. I have done the below activities 1. In each CPU station, I have made Scan Cycle load from communication to 50 %. 2. In SIMATIC S7 Protocol Suite system parameter setting for Cycle management removed tickmark for Cycle management by PLC. Regards, Amol G
Attachmentmerged.pdf (207 Downloads) |
|
Please rate it. |
|
| 9/20/2021 1:35 PM | |
|
Posts: 7298 Rating:
|
Hello AmolG, on the one hand, there is a known problem with https://support.industry.siemens.com/cs/de/en/view/109773812 On the other hand, have you installed the Simatic Net PC Software V16 ?
Georg Berghof |
This contribution was helpful to
|
|
| 9/20/2021 1:49 PM | |
|
Joined: 2/5/2013 Last visit: 12/22/2025 Posts: 330 Rating:
|
Hi Berghof, I have installed Simatic Net PC software V16. Just I will install Update 5. Can I install WinCC 7.5 SP2 from the below link https://support.industry.siemens.com/cs/ww/en/view/109783853 Regards, AmolG |
Last edited by: Jen_Moderator at: 09/21/2021 06:11:26Optimized link. Please rate it. |
|
Follow us on