9/15/2006 9:08 AM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating: (150)
|
What version of WinCC and Windows are you using ? If you have SP3 then you need to have hotfix 2 installed. It fixed a problem like the one you describe. The hotfix can be downloaded from this link : http://support.automation.siemens.com/WW/view/en/21480479 If this is not relevant then have you tried deleting the runtime data, if this is feasible ? Sometimes a corrupt alarm or tag logging database can stop runtime activating. |
9/15/2006 11:35 AM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating: (150)
|
Hi Duncan, Unfortunately V6 is not supported with XPSP2. You need at least V6 SP3 or SP4. You can see the compatibility matrix here : http://support.automation.siemens.com/WW/view/en/21927773 Again, these types of problems are common when using unsupported versions. Sorry. Salma |
9/15/2006 1:38 PM | |
Posts: 1275 Rating: (123)
|
Hi Duncan, You can order a free update for you v6.0 to v6.0 SP4 online at: https://support.automation.siemens.com/WW/skm/frameset.asp?url=%2FWW%2Fllisapi%2Edll%2F22303359%3Ffunc%3Dll%26objId%3D22303359%26objaction%3Dcsopen%26siteid%3Dcseus%26aktprim%3D0%26skm%3D1%26lang%3Den&Query=wincc+v6%2E0+sp4&SearchArea=downl&id=22303359&F11Marker=false&siteid=cseus&query2=&modelled=WinCC%3Bv6%2E0%3Bsp4&lang=en Also remember tocheck compatibility for theother siemens software you might be using. Best regards, Danielle |
11/16/2006 8:01 PM | |
Posts: 7 Rating: (0) |
hi duncan u try for this if u r having the previous backup ,load in pc and go to runtime hope this might solce ur problem |
Follow us on