2/14/2007 1:17 PM | |
Posts: 1275 Rating: (123)
|
Hey Óscar, Hereis a3D screens of ours.It's for a blast furnace'sgas washing system. Best regards, Danielle AttachmentAF1 - Lavagem de Gás.zip (431 Downloads) |
2/14/2007 1:26 PM | |
Posts: 19 Rating: (0) |
Here goes my first ever WinCC screen, just waiting for your (constructive[:P] ) criticisms! The buttons start the processes they represent, and blink in green while the process is in progress. The processes that need input parameters open "boxes" (pictures) to ask for them; the last box's OK button starts the process. The STOP button stops all processes but permits to continue them. If you want to terminate a process, you have to press the STOP button for 5 seconds. Oh, and thanks Danielle! [;)] Attachmentscreen1.zip (399 Downloads) |
2/14/2007 4:23 PM | |
Posts: 1275 Rating: (123)
|
Hi Óscar, We do have commands and parameter in ou system, but the command screen pops up when you click the desired object. I'm attaching one command window here. The top part opens up first, with state indication (e.g. open, closed) and commands, and indication of normal condition or failure, along with the reset button for the equipment. You can expand the box through the "+" button, and get access to filtered alarms for that equipment, and all interlocks for it. Interlocks in green are good to go, and those in yellow need to be satisfied to start the equipment. AttachmentComando.zip (319 Downloads) |
Follow us on