5/4/2012 10:42 AM | |
Joined: 4/19/2008 Last visit: 2/9/2024 Posts: 1525 Rating: (159) |
Also Some more for SIMITPlant simulation with SIMIT SCEmay be it will help you or other also..... |
Ammy |
|
5/4/2012 10:48 AM | |
Posts: 15 Rating: (0) |
Still nothing. When i change SimOn on 1 the Bad value is 1. |
5/4/2012 12:53 PM | |
Posts: 15 Rating: (0) |
As i wrote PV_out is 0. when SimOn is 1, PV_Out = SimPV_In |
5/8/2012 12:59 PM | |
Posts: 10 Rating: (0) |
If the PLC does not communicate to WinCC correctly, this is not linked to SIMIT. Please note that SIMIT does not connect to WinCC at all, but to the PLC only, using PROFIBUS and replacing the field. If there is a communication issue between SIMIT and the PLC, drop detailed description and required data to simit-hotline.industry@siemens.com |
9/3/2012 10:19 PM | |
Posts: 3 Rating: (0) |
Hello ny8 and Ammy, |
9/4/2012 8:48 AM | |
Joined: 4/19/2008 Last visit: 2/9/2024 Posts: 1525 Rating: (159) |
Hello DF, Can you tell me Which Version of SIMIT you have ? I have used From Old to new Version Also & I have no problem with F I/O, Try to Ack. the CH_XX Block after the SIMIT is in Runtime. Can You also Put the QBad Code you have ? |
Ammy |
|
9/5/2012 8:06 AM | |
Joined: 4/19/2008 Last visit: 2/9/2024 Posts: 1525 Rating: (159) |
Hello DF, Yes I have also do the same thing in for the Normal IO QBad, For Reset of the F I/O by F_Quit Block there is a Logic With Explanation, in the Following Manual SIMATIC Process Control System PCS7 Compendium Part B - Process Safety Page no 87 onword. but Exact the Reason Behind 6 & 9 to Ack. I also don't know...... |
Ammy |
|
Follow us on