3/2/2009 11:11 AM | |
Joined: 2/7/2008 Last visit: 9/24/2024 Posts: 15 Rating: (0) |
Hi Phantom75, Rebooted PC, stopped \\SCADA-PC01\WINCC-MSSQLSERVER (I hope this is what you meant wrt SQL)- still cannot add a tag. I have attached a print screen. Regards, AttachmentWinCC Tag logging problem.pdf (117 Downloads) |
3/2/2009 10:18 PM | |
Posts: 2661 Rating: (279)
|
Which computer is WINXP123? Is this computer trying to open the tag database on server? |
3/2/2009 11:30 PM | |
Joined: 2/7/2008 Last visit: 9/24/2024 Posts: 15 Rating: (0) |
This is the problem, I don't know where this computer is. The attachment shows the names of the computers that are on the network. XP123 is not one of them. Is it possible that it was a computer that previously was on the network but now has been removed. Is there any way that you can remove the write protection or a way to remove XP123.
AttachmentWinCC Tag logging problem 1.pdf (114 Downloads) |
3/3/2009 12:06 AM | |
Posts: 2661 Rating: (279)
|
From command prompt type net share and look for shares to this computer. If you find, delete share using net sharesharename /delete. |
3/3/2009 11:33 AM | |
Joined: 2/7/2008 Last visit: 9/24/2024 Posts: 15 Rating: (0) |
I have attached the results of the net share command.I could not find any link to XP123. Is there anything alse I can do?
AttachmentWinCC Tag logging problem 2.pdf (92 Downloads) |
Follow us on