11/27/2015 6:40 PM | |
Posts: 1 Rating: (0) |
Hello, I have quiet the same trouble... Logo!8 0BA8 and KTP400 basic panel. In the exemple : the Clock Synchronization of LOGO in http://w3.siemens.com/mcms/programmable-logic-controller/en/logic-module-logo/application-examples/Pages/Default.aspx In the WinCC project, when I select the "LOGO!" as the "communication driver", I can't affect the Global area pointer of HMI Device with this connection. The Connexion field stay in red with a message "This connection doesn't take in charge the area pointer of the operator panel" . And when I try with "SIMATIC S7 200" as driver connection, I can affect the global area pointer but nothing happens when i start the simulation, the date/time is the one of the panel and not the one of the logo!... If somedbody has any idea.... Is there any way to test the connection between the pannel and the Logo! ? Thanks in advance ------------------------------------------------------------------------------------------ |
Last edited by: neryoz at: 11/27/2015 6:42:46 PMLast edited by: Min_Moderator at: 11/30/2015 9:58:08 AMNew subject after splitting |
|
Follow us on