1/7/2016 8:41 AM | |
Joined: 7/28/2015 Last visit: 3/21/2024 Posts: 72 Rating: (1) |
Hello, I'm new here I have installed the winnCC TIA Portal to start to develope display pages of our HHO Hydrogen generator. Video demo here: https://youtu.be/MuV7WmEqG5U I found *almost* the all object to use for my system but I still can not find HOW to make a digital touch slider potentiometer. On
the current project I use a full complete channels LOGO8! PLC,
programmed with Confort 8. External I use one 0-10V 5K potentiometers
for editing in relatime the 10Kw powersupply to the Wet Cell HHO. In
attachment the Logo8 POT project picture. On the Ai3 is connected the 5K
Potentiometer to drive the two AQ1 and AQ2 outputs connected to the two
powersupply. Now I want to remove the analog 5K potentiometer and make all under display touch. On the WinCC TIA portal page, I found the all controls, like the Switch, Push, Bars....but no way to find HOW to create one rotatory or slider potentiometer. Is possible to get one example how to create this touch potentiometer and the variable to drive the AQ1 on Logo 8? Very thanks for the help! Domenik AttachmentPOT Logo8 Project.rar (192 Downloads) |
Follow us on