5/22/2012 12:42 PM | |
Joined: 9/28/2005 Last visit: 8/27/2024 Posts: 2957 Rating: (242)
|
(in english maybe ",Internal ERROR (details: Cannot find instance referenced by the relation).,1,0,12:11:56" ) This error occurs on a MP277 10" HMI connected in a complex network with a S7-300 PLC and others HMI. Only this HMI give me this error during compiling. I can't find how to solve. If i miss some information just ask. Regards Is it the same error whe you do 'Compile -> Software (Rebuild all)' ? If so then maybe good idea is to open Support Request Or maybe wait for other users with same issue to reply. As long as this is internal error, I think more help you can get at support request. |
Best regards, |
|
This contribution was helpful to3 thankful Users |
5/22/2012 12:55 PM | |
Posts: 6 Rating: (0) |
Is it the same error whe you do 'Compile -> Software (Rebuild all)' ? If so then maybe good idea is to open Support Request Or maybe wait for other users with same issue to reply. As long as this is internal error, I think more help you can get at support request. Solved as Darius suggested. Thank you!
|
5/22/2012 1:45 PM | |
Joined: 9/28/2005 Last visit: 8/27/2024 Posts: 2957 Rating: (242)
|
Solved as Darius suggested. Thank you! You mean you send to support request or 'Compile -> Software (Rebuild all)' help you ? |
Best regards, |
|
5/22/2012 2:28 PM | |
Posts: 6 Rating: (0) |
Sorry,'Compile -> Software (Rebuild all)' solved all! |
This contribution was helpful to1 thankful Users |
3/11/2013 9:49 AM | |
Posts: 1 Rating: (0) |
Sorry, i am a fresh man ,could you tell me the meaing of "Compile -> Software (Rebuild all)" |
10/4/2019 7:25 AM | |
Posts: 3 Rating: (0) |
hello , it really solves when you rebuild all, thanks |