(0)| 1/28/2021 7:45 PM | |
|
Posts: 1 Rating:
|
hello; I need your help about card MMC 6ES7953-8LP31-0AA0, the PLC dosent read it when I put it . I tried format it with soft WinHex but without success thank you ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/29/2021 09:46:21New subject after splitting |
|
| 2/2/2021 10:52 AM | |
|
Joined: 3/11/2019 Last visit: 10/15/2025 Posts: 1653 Rating:
|
Hi, please note the informations from following FAQ: "If an MMC of the S7-300 CPUs is used for non-SIMATIC purposes or is formatted in a third-party device, then the internal structure of the MMC is overwritten and cannot be restored. In this case the SIMATIC CPU no longer recognizes/accepts the MMC. It is then no longer possibleto use this MMC in a SIMATIC CPU." Why is the MMC no longer recognized by SIMATIC devices after it has been formatted in a third-party device?
regards |
|
Feedback appreciated, please rate |
|
| 2/4/2021 5:30 AM | |
|
Joined: 5/28/2008 Last visit: 10/23/2025 Posts: 4522 Rating:
|
Hello, Forget it! Because when tring to format using third party programs, it defected the MMC. and you have to purshase a new MMC. But tell us also Part no. of CPU. How do you format or reset an MMC (Micro Memory Card) for SIMATIC S7-300 CPUs? |
|
Ayman Elotaify |
|
Follow us on