Industry Online Support
Technical Forum
12/23/2019 8:16 PM | |
Joined: 9/23/2005 Last visit: 3/11/2024 Posts: 4325 Rating: (1415) |
“Simple Samples” are small projects that demonstrate simple features. The target is giving a quick overview about the theme and be used as start point for related discussions. Follow there are a short description and the configuration main steps. Description: On each 2 seconds time interval a script is called. In this example the script increment a TAG. Configuration main steps:
Project (.zap16 ziped as .zip)
AttachmentCallScriptByTime.zip (503 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to1 thankful Users |
Follow us on