11/10/2020 2:33 PM | |
Joined: 9/23/2005 Last visit: 4/29/2024 Posts: 4325 Rating: (1425)
|
Hi, “Simple Samples” are small projects that demonstrate simple features. The target is give a quick overview about the theme and be used as start point for related discussions. Follow there are a short description and the configuration main steps. Description: It is possible to open / close (show / hide) a screen windows by an external button acting on its visible property. It could be done for different ways (e.g. by a tag or script). Attached a simple program that demonstrate that. AttachmentProject1_20201110_1025.zip (745 Downloads) |
Last edited by: Denilson Pegaia at: 11/10/2020 15:31:12Denilson Pegaia |
|
This contribution was helpful to2 thankful Users |