12/12/2019 3:06 PM | |
Joined: 9/23/2005 Last visit: 4/17/2024 Posts: 4325 Rating: (1419)
|
“Simple Samples” are small projects that demonstrate simple features. The target is giving a quick overview about the theme and be used as start point for related discussions. Follow there are a short description and the configuration main steps. As from the TIA V16, there was the introduction of the WinCC Unified. This is an engineering platform for HMI Comfort Unified and for WinCC Unified PC. It brings many news regarding the WinCC Advanced / WinCC Professional. Definition / characteristics Technological Hierarchy is a new way to manager (organize/navigate) objects (e.g. Faceplates / screens). In the Technological Hierarchy, the programmer defined a “folder structure” that is used to navigate in de screens / filter the alarms in runtime. It substitutes the navigation configuration on the HMI’s creation wizard and add an alternative to do it in SCADA systems. After some configuration steps, the navigation is ready for use, without the necessity to use individual navigation buttons on the screens. Changes after the original creation could be done without effort. The Technological Hierarchy could be configured in the Plant Object view (a new tab on project tree, on right side of the Devices tab). It is possible to create different Plant views (Technological Hierarchy) and assign then to different HMI devices in the project, so that the different HMI’s could have independent plant views. Prerequisites: Define the objects on PLC side: define PLC (HW, networks, etc.), PLC Data type and the variables (e.g. instance DB’s) using these PLC Data Type. Create / configure respective faceplates on the HMI side (see steps in "WinCC Unified – TIP’s for Faceplate" https://support.industry.siemens.com/tf//ww/en/posts/wincc-unified-tip-s-for-faceplate/225140/?page=0&pageSize=10) Configuration sequence:
TIP on operation: on the Plant Overview control, there is a combo box (open, right), that filter (all folders, folders with defined screens, folders with active alarms). if you don't find a folder online, check if the selected filter matchs. AttachmentTechnological Hierarchy_20200223_0953.zip (932 Downloads) |
Last edited by: Denilson Pegaia at: 12/12/2019 15:10:01Last edited by: Denilson Pegaia at: 02/24/2020 16:15:01Denilson Pegaia |
|
This contribution was helpful to3 thankful Users |
Follow us on