Industry Online Support
Technical Forum
12/26/2019 2:14 PM | |
Joined: 9/23/2005 Last visit: 4/29/2024 Posts: 4325 Rating: (1425) |
Hi, “Simple Samples” are small projects that demonstrate simple features. The target is giving a quick overview about the theme and be used as start point for related discussions. Follow there are a short description and the configuration main steps Trends Companion is an object that complement the visualization of a Trend object, diplaying in tabular format detailed / processed data TIP: Trend companion objects should work linked to Trend Objects. An exeample of how to configure Trend objects is showed in the post "WinCC Unified – Simple Sample - Trends (time based)" (https://support.industry.siemens.com/tf//ww/en/posts/wincc-unified-simple-sample-trends-time-based/226107/?page=0&pageSize=10). Configuration main steps:
TIP: The Trend companion object has 3 modes: Rules, static area, static results. When the user open the screen, the object came with the mode defined on Properties -> General -> Trend companion mode. The mode could be selected online by this own buttons. To set these buttons visible: Object properties: miscellaneus -> Toolbars -> Elements -> [0] Button / [1] Button -> Visibility = true. TIP: the mode static area just will work if a time range would be selected in the Trend Object. To activate this, a button on the trend object should be enable: properties -> Miscellaneous -> Toolbar -> Elements -> [18] Button (Define statistic area) -> visible = true TIP: the mode static resultsjust will work if a time range would be selected AND the calculation is triggered in the Trend Object (not in the trend companion). To activate these, a button on the trend object should be enable: properties -> Miscellaneous -> Toolbar -> Elements -> [18] Button (Define statistic area) / [19] Calculate statistic -> visible = true Project (.zap16 ziped as .zip)
AttachmentTrendsCompanion.zip (529 Downloads) |
Last edited by: Denilson Pegaia at: 11/16/2020 11:16:03Denilson Pegaia |
|
This contribution was helpful to1 thankful Users |