11/15/2011 11:33 PM | |
Posts: 6 Rating: (0) |
Hi, On WMVare Workstation I have WinXP Pro with WinCC V11 SP1 Professional. I migrated project from WinCCflexible 2008SP2 toWinCC V11.I used to transfered project to MP377 HMIfrom WinCC flexible2008 using MPI/DP Mode (in set PG/PC interface I had set NetLink Pro ETH(MPI) driver - to transfer project using this converter (www.softing.com)). But in WinCC V11 project (migrated or a new project) when I make Download to divice in Extended download to device window in Type of the PG/PC interface selection isn't MPI/DP interface. It is possible to transfer project from WinCC V11 Pro to MP377 using MPI conection? |
11/17/2011 12:41 PM | |
Posts: 6 Rating: (0) |
So, it means that WinCC V11 don't have the possibility for downloading the project to MP377 using MPI/DP connection? |