2/25/2014 7:57 PM | |
Posts: 25 Rating: (0) |
Second attachment |
2/26/2014 10:10 AM | |
Posts: 25 Rating: (0) |
WinCC V12 http://cache.automation.siemens.com/dnl/TI/TI4MTk5MDcA_68075405_HB/WinCC_Advanced_V12_enUS_en-US.pdf Page 1682. S7-1200 is supported. The follows address types are supported: ● IP address ● MPI address The follows PLC types are supported: ● SIMATIC S7 1200 ● SIMATIC S7 300/400 ● SIMATIC S7-NC ● SIMOTION |
2/26/2014 12:56 PM | |
Joined: 11/15/2006 Last visit: 5/7/2021 Posts: 1319 Rating: (170) |
ChangeConnection is not possible with S7-1200 as far as I know, but: it might be dependend on the FW version of the RT / Panel, as in V11 it was possible, at least as far as I remember. Check the online help and readme, I thought there was entry telling that is is not possible with S7-1200. |
Have Fun! |
|
10/2/2015 11:51 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
New question published by Danilo Barbosa is split to a separate thread with the subject WinCC V13 SP1 RT Professional, ChangeConnection. Best regards |
Follow us on