Industry Online Support
Technical Forum
1/15/2014 7:25 PM | |
Posts: 311 Rating: (3) |
Hello, Can not do that, becuase I only have the runtime environment in the other computer. Regards Per Olof |
1/16/2014 7:26 AM | |
Posts: 1299 Rating: (135)
|
Hello, are the engineering and runtime pcs in the same network? you have to download it just as you're doing when loading a panel or plc... K!ke |
1/16/2014 8:22 AM | |
Posts: 311 Rating: (3) |
Hello, No, not on the same network. Is it not possible to move files instead of "download" ? Regards Per Olof |
1/16/2014 9:53 AM | |
Posts: 1299 Rating: (135)
|
Hello, there is a way to transfer it manually, but this way is complicated. if there's no way to connect the pcs you can ask siemens hotline how to transfer the project. K!ke |